NX Minimum Requirement for using Staged Model application in TC Integration

2022-10-03T10:43:30Z
NX for Design

Summary


Details

Why is Staged Model application not available in TC Integration mode of NX?


What is the minimum requirement for using Staged Model application in Teamcenter Integration?

Solution

Minimum Software requirement:

TC13.1

AWC5.2

NX1980

In addition, the nxb0Stage template needs to be installed. This is done via TEM by toggle on "NX Stage Model"



KB Article ID# PL8676123

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX