How to use Selection Prediction to select multiple entities

2024-02-21T17:12:17Z

Summary


Details

How to use Selection Prediction to select Multiple entities.

Solution

See the attached video for the procedure to use Selection Prediction to select multiple entities along with the provided steps below.

How to Use Selection Prediction to Select Multiple Entities

NX93100 NX Mach 3 Product Design or NX93300 NX Mach 3 Industrial Design is required to access this functionality.

1.       Open part and choose the desired command, i.e. Edge Blend.

2.       Select a feature edge.

-          Note: The edges highlighted in blue are the predicted edges.

3.       In the Selection Scene Bar, choose Border Bar Options -> Selection group and ensure Selection Prediction Options Group is turned on.

4.       To change the sensitivity, in the Selection Scene bar click Selection Prediction Options with your feature still highlighted.

5.       Adjust the slider as necessary.

-          Note: Left increases sensitivity, right decreases sensitivity.

6.       Once the desired edges are highlighted in blue, in the Selection Scene Bar click Select Predicted Objects.

7.       In the command dialog box, click Ok.

KB Article ID# PL8675843

Contents

SummaryDetails

Associated Components