Legacy Hole Table - Origin / Size

2022-10-11T18:09:43Z

Summary


Details

Recently upgraded from ST5 to 2022, and would like to know if there was a way to still use the ST5 Hole Table functionality.

Platforms
  • na windows-1032
Release Versions
  • Solid Edge V222MP8
Solution

o In Draft, click the "Customize" button on the Quick Access Bar at the top of the Solid Edge application window.

o Select the "All Commands" option from the "Choose commands from:" dropdown list.

o From the "Quick Access" tab, select "Legacy Hole Table" from the list, then "Add" so that it appears on the Quick Access toolbar

o This will create a new Theme that will need to be applied to get the prior functionality.

You can now use the old method for the Hole Table used in ST9 and prior.

Notes

KB Article ID# PL8675592

Contents

SummaryDetails

Associated Components