Create Real PMI Objects from Neutral Files Formats.

2023-09-21T14:53:54Z

Summary


Details

When importing a file from other software into NX software, some PMI information changes.

In this example, the information was represented with the diameter symbol and is now represented with the text “DIA”.

Information displayed in Catia software:


Information imported into NX software:


Release Versions
  • NX V12.0.2
Platforms
  • Windows x64 10
Solution

Deactivate the "Create Real PMI Objects from Neutral Files Formats" option.

File -> Utilities -> Customer Defaults -> PMI -> PMI General -> Miscellaneous;


KB Article ID# PL8675499

Contents

SummaryDetails

Associated Components