How to Create a Break Out Section View in Drafting

2024-02-21T17:11:53Z

Summary


Details

 How to create a break out section view in drafting.

Solution

 See the attached video for this procedure along with the provided steps below.

How to Create a Break-out Section View in Drafting

1.       Select desired view border and right click.

-          Note: If the draft only has one view, a second will have to be created in order to indicate how deep the section view should go. The second view can be deleted after the section view is created.

2.       Click Active Sketch View.

3.       Using the options in the Sketch tab -> Sketch group, create the boundary lines that will make the break-out section view.

4.       When finished, choose the Sketch tab -> Sketch -> Finish Sketch.

5.       In the Top Border Bar, choose Menu -> Insert -> View -> Break-out.

-          Note: For a more detailed explanation of the Break-Out Section View dialog box, visit Drafting (siemens.com)

-          For exceptions, visit Drafting (siemens.com).

6.       Select the view that the break-out section will be in.

7.       On one of the views, select a base point.

-          Note: This indicates how deep the section view will go.

8.       Select the boundary lines.

-          Note: Ensure that the thin white line connecting the two curves doesn’t intersect them.

9.       Click Ok.

-         

Notes

   Note: For more details, visit this link: https://docs.sw.siemens.com/en-US/doc/209349590/PL20230425446868577.drafting/views_view_breakout_op

KB Article ID# PL8674706

Contents

SummaryDetails

Associated Components