UG_PART_ATTRIBUTE form is not getting generated under the UG_PART dataset

2022-12-23T11:25:34Z

Summary


Details

Question on the UGPART-ATTRIBUTE form.This form is not getting generated under the UG_PART dataset when the data is saved from NX, and because of that unable to read the Drawing part attribute values in Teamcenter when stored from NX. Need to enable the Part attribute form under the UGPart data type named reference

Platforms
  • na windows-1032
Release Versions
  • NX V1953
Solution

Users can try editing the TC preference

TC_NX_nonmaster_additional_forms: Add UGPART:UGPART-ATTRIBUTES.This helped to get the attributes in TC from NX UGPart dataset.

Notes

KB Article ID# PL8674676

Contents

SummaryDetails

Associated Components