Few components are not visible in the assembly BOM
From the Test assembly, we could see the presence of the variable "PLIST_IGNORE_MEMBER=1" that was not allowing the component to be part of the Assembly BOM list.
Once the variable was removed from the Non-Bom component the same can be seen appearing in the Main Assembly BOM list.
Notes