A Floor Wall operation is created to rough a notch. The operation will be set up to cut in both the Climb and the Conventional directions. The setting Containment -> Open Path -> Open Passes -> Alternate Cut Direction needs to be enabled to do this. The option is missing in the Floor Wall operation, though. How can this option be turned back on?
The Main -> Cut Pattern -> Follow Part option must be selected for the Alternate Cut Direction option to be visible.
When set the Alternate Cut Direction option will become available.
Notice the Climb and the Conventional tool motion as seen in the picture below.