Curves are not connected error joining curves using Composite Curve.

2022-09-19T18:41:30Z

Summary


Details

User broke up a curve into 200 segments and now wants to get the curves back to a single curve. Attempting to Join the curves using the Composite Curve tool with the Curve Rule set to Tangent Curve the option fails with error that the curves are not connected.

Solution

The following steps can assist the user to find the problem area to make adjustments or fix the area. The problem may be caused by overlapping curves.

- Change the Curve Rule to "Single Curve" and then select 2 curves and verify that the curves will join.

- If the curves Join, select Undo.

- Try to select the curves by using a rectangle around half of the curves.

- If the curves Join, try the other half.

- Keep performing this step to narrow down the problem area.

KB Article ID# PL8673262

Contents

SummaryDetails

Associated Components