About Drafting shortcut keys

2022-09-16T08:48:57Z

Summary


Details

If you look, between NX12 and NX 1953 and the advanced version of NX, a few shortcuts have disappeared as L for Line, O for a full circle, S for Spline, and P for Polygon, etc.

Solution

User Interference is changed from NX1953 the shortcut keys are assigned to the constraints.

L for Make Perpendicular.

O for Make Tangent.

S for Make Symmetric.

P for Make Parallel.

Refer to the below image for more info.


We can set the default setting by customizing it. Refer to the below screenshots and steps,

Steps:

-----------

1. Drafting Application select Customize.


2. Select; Keyboard.


3. Set Shortcut to use Application Only and press "L " as shortcut key>Assign.



4. Shortcut key L is set for a Line command.


-----------------

KB Article ID# PL8672113

Contents

SummaryDetails

Associated Components