Solid Edge Solid Edge 2022 - Maintenance Pack 9 Announcement

2022-09-12T16:34:18Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

September 12, 2022

Dear Solid Edge Customer:

Solid Edge 2022 Maintenance Pack 9 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2022 MP9

Version: 222.00.09.06

Solid Edge 2022 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

Support Center: https://support.sw.siemens.com

Solid Edge 2022 MP Download Area: https://support.sw.siemens.com/product/246738425/download/PL20200902110958364

Note: if the MP download area URL doesn't work with your browser, please navigate from the top-level Support Center.

======================

Operating System Update:

======================

In addition to the Operating System Requirements documented in the original Solid Edge 2022 readme,

Solid Edge 2022 MP2 is now certified to run on Windows 11 Enterprise or Professional (64-bit only).

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Maintenance Packs, navigate to your Support Center profile:

https://account.sw.siemens.com/profile, scroll down to Newsletter Subscriptions, then check the box for 

Software Field Bulletin

============================================

This Maintenance Pack addresses the following PRs:

============================================

===Assembly===

PR 10235622: Circular dependency error when creating relationships

PR 10303168: Creating a second feature on a Frame causes the first feature on the Frame to fail

PR 10404066: Solid Edge crashes while opening a specific assembly document

PR 10354423: New Frames disappearing after editing existing Frames

PR 10407894: Changing an unrelated hole feature value is causing the finite depth to revert

PR 10362559: Can't create a frame with mixed 2D and 3D Sketches.

PR 10373738: Some Frames in subs disappear from the screen on file open

PR 10420156: Axial Align unlocking rotation after undo

PR 210763: Unable to create/update assembly features

===Draft===

PR 10394706: Session does not respond anymore after entering a value for a linear dimension

PR 10229076: Create 3D does not have any templates available

PR 10393437: Contents explode after unblocking and moving objects

PR 10304017: Experiencing multiple crashes per day

===General===

PR 10377203: Random aborts when Windows 'Use text cursor' setting is "On".

PR 10378769: Hardware Part field missing in files created in SE V11

PR 10408060: Custom properties deleted when part transformed to sheet metal

===Part/Profile/Sheetmetal===

PR 10304484: Can't copy Sketch with conical curve created in Draft to part or PSM files

PR 10406495: Aborting using Inquire Element while changing variable

PR 10140212: Solid Edge crash when opening specific psm file

PR 8610042: Some items are displayed twice in the File Properties dialog

PR 10423391: Reproducible crash when editing Chamfer

PR 201156: Solid Edge hangs when modifying a Bolt hole circle

===Solid Edge Data Management===

PR 10398496: where used pops up when using "open draft."

PR 10449224: BIDM workflow causes Available files to become Read-Only for customer

===Teamcenter Integration for Solid Edge===

PR 10322359: Default Template wrong linking in User Interface

PR 203073: TC13.3 Integration for SE222

===Translators===

PR 10389672: Solid Edge crashes when translating to STEP if the Part file is empty

PR 10385320: Crash while opening DWG file into Solid Edge

KB Article ID# PL8671715

Contents

SummaryDetails

Associated Components

SE_BETA