Can’t create multiple frames using same path.
SolutionThis could be because ‘Ignore entity if frame already exists’ is checked in Frame Options dialog box.
If this is checked then If any frame member is already created on the entity selected in the Select Path step, then that entity is ignored when creating the frame. Unchecking this allows to create multiple frames using same path.