Currently ‘Highlight NX objects’ command in PMI report works for only the work view.
How to highlight PMIs that are placed in other views?
SolutionIn the latest versions, if the user creates an MBD query to display the PMIs of multiple views and creates a model view based on the results of the query , then it is possible to highlight them using ‘Highlight NX objects’ command from the PMI Report( MS -Excel Add-in)