NX NX Mach Bundle ID Conversion

2022-09-28T13:07:58Z
NX System Administration

Summary


Details

Dear NX Customer:

As part of our ongoing commitment to you to deliver the highest quality products to you, we regularly look at how the NX product is packaged and delivered. In 2020 we decided to remove redundant license bits from the NX Mach licensing. This makes the license file easier to understand by removing unused entries.

To allow us to track the initial implementation and adoption the decision was made to use new part numbers and flag the original NX Mach products as legacy products.

Now two years on we have decided to automatically move all customers to the new part number scheme.

The purpose of this SFB is to be sure that you are not surprised by this change when you receive a new license file.

For most customers, the timing of this change is being coordinated by your local team to coincide with regular maintenance renewal schedule. Further details will be provided at your renewal time.

For some customers, this change could happen at an earlier time. Specifically anytime you make a change that results in a new license file being generated for your site. This would be the case if you were to request a Trial product be added to your license or if you need to move your license to a new server.

 In all cases, the result is you will see legacy product IDs transition to current product IDs while the core NX product capabilities remain the same.

Action for Users:

The only impact you should notice is that the text string used to identify your Bundle when running NX will change, because it based on the product ID.

For those who use the interactive Licensing Tool GUI to set your Bundle, you will need to re-select your appropriate Mach bundle by name.

For those who administratively set bundles using either the Windows environment variable (UGS_LICENSE_BUNDLE) or a Windows Registry key value (NX_BUNDLE, set via the Licensing Tool), you can programmatically set the value to be both the old and new values so that your clients can easily adapt to the new license file.

For example, if your value was previously "NX11100N" (for NX Mach 1 Design) you would use "NX11100N, NX91100".

If you previously used 2 bundles, such as "NX11100N, NX13100N" (for Mach 1 Design and Mach 3 Product Design) you would use "NX11100N,NX13100N,NX91100,NX93100".

For reference, here are the mappings for Product (and bundle ID's) that are changing. In most cases, the change consists of the leading "1" changed to a "9".

Product / (Bundle Id) Name New Product / Bundle Id
NX10107 NX Layout NX90107
NX11100 ( NX11100N) NX Mach 1 Design (Node Locked) NX91100
NX11110 NX Mach 1 Design (Floating) NX91110
NX12100 NX Mach 2 Product Design NX92100
NX13100 (NX13100N) NX Mach 3 Product Design NX93100
NX13200 NX Mach 3 Mold Design NX93200
NX13210 NX Mach 3 Progressive Die Design NX93210
NX13300 NX Mach 3 Industrial Design NX93300
NX14112 NX Mach 4 Marine Craft Design NX94112
NX11113 Mechatronics Concept Designer NX91113
NX12300 NX Cool Shape Design Bundle NX92300
NX13110 NX MACH 3 Additive Design with Convergent NX93110
NX30437 NX CAM Mach-level Data Management Add-on NX90437
NX12411 NX Mach 2-E Advanced Machining NX11490
NX13420 NX Mach 3 - Advanced Machining NX12490
NX14100 NX Mach 4 High Tech Design NX94100
NX14110 NX Mach 4 Ship Design NX94110
NX14111 NX Mach 4 Ship Design NX94111

Conclusion:

Users with NX Mach 3 Product Design or NX Mach 3 Industrial Design will see new capabilities with the addition of Artificial Intelligence-driven features such as select similar. These capabilities are NOT in the legacy products.

NX Design product line has a foundation in a core scalable seat, which can be ordered as NX Mach 1, NX Mach 2, or NX Mach 3.

The result of this work means that the current product IDs for the core design solid modeling seat are:

  • NX91100 NX Mach 1 Design (Node Locked)
    • NX91110 NX Mach 1 Design (Floating)
      • NX92100 NX Mach 2 Product Design
        • NX93100 NX Mach 3 Product Design

          NX offers a range of integrated optional product modules that can be ordered individually, or as the NX Value Based Licensing package.

          The current product IDs for the optional integrated modules are:

          • NX35050 NX Value Based Licensing pack for 50 Tokens
            • NX35100 NX Value Based Licensing pack for 100 Tokens

              There are over 100 NX product IDs for optional modules that are also current

              Current product IDs benefit from continuous product enhancement updates.

              For more information on NX and or any questions regarding product IDs, please contact your local Siemens Sales representative, Siemens Support Center, or Reseller who can assist or put you in contact with our Product Management team.

              Respectfully,

              George L Rendell

              Vice president, NX Design product management

              Siemens Digital Industries Software

              KB Article ID# PL8670765

              Contents

              SummaryDetails

              Associated Components

              Licensing