How to choose dataset and relation type while exporting a step file

2022-09-07T08:55:26Z

Summary


Details

Often customers ask if it is possible to choose the dataset and relation type for the dataset created by an export operation performed on a step file

Solution

The procedure to choose dataset and relation types is described in the product documentation, in the following pages:

Exporting to Teamcenter

https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20191127135844554.dataexchange/html/xid1676865

Teamcenter preferences for exporting and importing datasets

https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20191127135844554.dataexchange/html/xid1676860

The TC_NX_DataExchange_Dataset_Preference must be set according to the desired result and the syntax described in the documentation.

Here is an example:


Also, the parameter REF_TYPE, in the BMIDE, should have the same value as in BMIDE in the references table of the specific dataset.


After having set these preferences, the new dataset type and relation should be available in the STEP Export window in NX.

In some NX versions there may be a refresh issue in the Export window.

In order to overcome the problem, the user should select “Filesystem” and once again “Teamcenter”, in the field "Output file destination", then the window should update the content with the correct data.

KB Article ID# PL8670671

Contents

SummaryDetails

Associated Components