NX Usage of item revision "00" in tabular notes

2022-09-07T08:54:50Z
NX for Design

Summary


Details

When compiling a tabular note, if the text to insert is the revision of the item and the revision is "00", the inserted text is wrong.


If the revision is 01 or A or B or anything else the text is inserted correctly. But if the Revision is “00” then a dash is inserted in the cell.


Solution

A setting is available to control the zero display. Zero value can be displayed as Zero, Dashed or Empty. As revision has value 0 it shows the display based on this setting. Here to display as 00 go to MB3->Settings on cell and Change Common->Cell->Zero Display to Zero.


KB Article ID# PL8670661

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX