Edge associated with PMI Note in 3D PDF is not highlighted

2022-09-05T03:40:53Z

Summary


Details

Even if opening 3D PDF exported by TDP with Acrobat Reader and select PMI Note, the related edge is not highlighted.

Reproduced Steps:

1. Create one edge as "Associated Objects" when entering PMI Note


2. PMI tab > Publish > 3D PDF > OK


3. Open the exported 3D PDF with Acrobat Reader

*** The associated edge cannot be highlighted even if PMI Note is selected.


Solution

The behavior is working as designed.

Notes

Faces and bodies with associated PMI Notes are highlighted, but edges are not supported due to functional limitations.

The same is true for all PMI geometries such as Feature Control Frame, Datum Target and Balloon, edges are not highlighted.

*** Please refer to PL8670348 for Japanese article.

Platforms
  • Windows x64 10
Release Versions
  • NX V1953
Release Versions
  • Teamcenter Visualization V13.1

KB Article ID# PL8670349

Contents

SummaryDetails

Associated Components