CheckMate "Check Fully Defined Sketch" checker does not detect fully constrained sketches

2022-09-05T03:35:33Z

Summary


Details

In order to check whether the sketch created by old style sketch in NX 2206 is fully constrained, I used the "Check Fully Defined Sketch" checker, which is a new function of NX 2206, but even though the sketch is fully constrained, it is detected as "Skipped" instead of "Passed" in the "Result" column.

Reproduced Steps:

1. Prepare a fully constrained sketch created in old style Sketch

2. HD3D Tools Tab > Check-Mate > Set Up Tests > Tests > ①Check Fully Defined Sketch > ②Add to Selected > ③Run Checkmate Test


3. Confirm the result

*** It will be detected with “Test status is Skipped”, not be detected with “Passed”.


Solution

The behavior is working as designed.

This checker is for new style sketches only, not for old style sketches.

Excerpt from the documentation:

Skipped - The work part has no sketch or contains only legacy sketches.

Notes

For more information about this checker, please see "What's New in NX 2206" - "Check-Mate"/"Validating sketches in a work part".

https://docs.sw.siemens.com/ja-JP/product/209349590/doc/PL20200605195244930.whatsnew/html/xid2054674

*** Please refer to PL8670339 for Japanese article.

Platforms
  • Windows x64 10
Release Versions
  • NX V2206

KB Article ID# PL8670341

Contents

SummaryDetails

Associated Components