NX crashes when creating flange in Sheet Metal

2022-09-05T03:32:36Z

Summary


Details

After generating a new body using Cleanup Utility command, NX crashes when trying to create a flange to the body.

Reproduced Steps:

1. Prepare a sheet metal model by using “Tab” and “Bend” commands

2. Create a new body by using “Cleanup Utility” command



3. Select an edge on the side with the bend by “Flange” command


Solution

The behavior is due to NX bug and occurs in NX 1926 – NX 2006. It is currently under investigation, so Siemens will keep you informed through this article about updates such as the fix or others.

Notes

Occurrence condition : If the following two conditions are met.

1. There are one or more bends in the body generated by the Cleanup Utility

2. Choosing edge on side with bend by “Flange” command


Note: The same phenomenon also occurs when using the "Cleanup Utility" on the sheet metal created by "Contour Flange" or "Lofted Flange".

*** Please refer to PL8670321 for Japanese article

Platforms
  • Windows x64 10
Release Versions
  • NX V2027

KB Article ID# PL8670323

Contents

SummaryDetails

Associated Components