Checking 'Properties' of 'Measure' feature outputs internal error

2022-09-05T03:28:49Z

Summary


Details

In the Assembly environment, when checking "Properties" of "Measurement" feature created in a work part, an "Internal Error: Memory Access Violation" occurs.

Reproduced Steps:

1. Assembly*1, Component*1(with a simple solid)

2. Make the comp work part

3.  “Analysis” > “Measure”

      -  Select “Associative” and “Display Annotation” option


4. Select “Measure” feature > click the mouse right button > “Properties”


Solution

The issue was occurring in NX 1872 and higher.

The behavior is due to NX bug and is fixed in NX 2212.

Workaround:

Do NOT check "Properties" in the state of a work part, switch to the display part (such as making use of "Open in window") and check it.

Notes

Occurrence condition: Occurs when the following two conditions are met.

1. Created by “Associative” and “Display Annotation” options

2. Check "Properties" in working part (in assembly environment)

* The problem is in the "Properties" command. "Measure" feature which is created has no any problem and can be used with confidence.

Error Message : Either of the two errors is output depending on the situation.

Internal error: memory access violation


Bad tag error.


*** Please refer to PL8670316 for Japanese article.

Platforms
  • Windows x64 10
Release Versions
  • NX V2007

KB Article ID# PL8670317

Contents

SummaryDetails

Associated Components