Teamcenter When exported a report to PowerPoint it gets exported with file type as "File".

2022-08-20T05:30:59Z
Reporting and Analytics

Summary


Details

When exported a report to PowerPoint it gets exported with file type as "File".

Below is the screenshot 

TcRA 14 Exported PowerPoint file and type is file which is incorrect

TcRA 13 exported PowerPoint file and type is Microsoft PowerPoint Presentation is the correct extension 


Solution

When there is no extension to a file, it gets downloaded as file type 'File'.

Check the database entry for the PowerPoint using the following sql

SELECT * FROM EQUBE_PROPERTIES where PROPERTY_NAME='powerpoint-file-format'

Output of the command should be similar to the following 


If the user is getting the output as above then change the PowerPoint File format to PowerPoint 2007 Presentation


KB Article ID# PL8666600

Contents

SummaryDetails

Associated Components

Reporting and Analytics