Tecnomatix Process Simulate compatibility with Active Workspace 6.1 or higher versions

2022-08-16T08:11:05Z
Process Simulate

Summary


Details

Active Workspace 6.1 has stopped supporting Internet Explorer, and therefore
in order to use TCMA 6.1 and higher versions with Process Simulate,
Microsoft Edge will be used with TX2206 (and higher versions).

Note for TX2206:

When using Active Workspace 6.1 or higher versions with Tx2206, the
following should be performed for successful TcMA integration:

Validate that MS Edge is installed on the client machine

Install Tecnomatix_client_hotfix_2206.0000.0004. 
See Tecnomatix_2206.0.x_Additional_Information_AUG_15_2022.pdf for
instructions.

Note:
Tecnomatix versions prior to Tx2206 are not compatible with TcMA 6.1 and
above.

Tx2206 still supports previous versions of AW based on Internet Explorer

KB Article ID# PL8666564

Contents

SummaryDetails

Associated Components

Process Simulate Installation