Can we modify the view below in AW 5.x or AW 6.x?
This does not appear to be editable via the XRT Editor in
Active Workspace.
This is the only preference that seemed applicable to the
Board at all:
I tried using "export_uiconfig" to modify some column information, but did not see any changes in the Board view. I have used this utility successfully to make other column changes.
Currently, there is no way to add or modify columns for Board View (Schedule Tasks). This is not supported in AW 5.x or AW 6.x. An ER could be submitted if so desired.