Tecnomatix Chinese characters in OLP command

2022-08-23T07:52:59Z
Process Simulate

Summary


Details

When import style01.ls (I have Process Simulate 16.1, Fanuc-Rj  version 3.17 installed), if the program has Chinese characters, it will become garbage characters; But when open OLP command and copy/paste, it displays correctly. Customer have to copy/paste again after importing.

Customer suppose the Chinese character can be supported in "OLP command", and hope this issue can be fixed, he does not need copy/paste the program again after importing program.

Solution

A new combo box in Download Settings dialog enables selection of the encoding to be used.Implemented in Fanuc RjLib 3.72 and FanucRj 3.44

Notes

KB Article ID# PL8665780

Contents

SummaryDetails

Associated Components

Process Simulate Off-Line Programming (OLP)