Teamcenter Unable to perform runTcFTSIndexer.bat -task=objdata:savedquery

2022-08-14T17:50:43Z
Active Workspace

Summary


Details

Trying to reindex single part through runTcFTSIndexer.bat -task=objdata:savedquery but getting a below error

java.rmi.RemoteException: Type objdata Flow sync is already running. Only one objdata flow can be run at any given time.

Solution

Objdata index only supports one flow at any given time. You should not run multiple objdata flows at the same time. The best practice is to perform one-off indexing like objdata:index or objdata:savedquery separately and then once they are done, run the normal sync flow.

KB Article ID# PL8665246

Contents

SummaryDetails

Associated Components

Active Workspace - Indexing and Search