Dialog box to save a part in Teamcenter Solid-works interface takes too long time
SolutionThe root of the problem is the Server Manager is hosted on a machine using IPv6, and is not properly configured for that.
As a work-around the Server Manager configuration can be adjusted to account for this, modify these files under pool_manager/confs/XXX/
1. mgrenv.bat
2. tecsenv.bat
3. Remove “-Djava.net.preferIPv4Stack=true” from the JVM_OPTS.
4. Restart the Server Manager, if the Server Manager is installed as a Windows Service, the Windows Service must be re-installed