Not able to Create/publish technical data packages in batch mode in a Teamcenter integrated NX, in NX2206 version.
While executing the batch mode utility in a Teamcenter integrated NX, below error is displayed.
"Error: -login_file argument not defined"
Starting from NX 2206, a login file is required to run the TDP batch utility in Teamcenter mode.
The arguments have been also modified.
This information has been updated from NX2206.3000 downloads.
Please download the latest TDP files from the NX2206.3000 downloads.
https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200605195244930.xid1753866/html/xid2092068?audience=external
Ensure to set the TC parameters to connect with the database in the command prompt used.