Teamcenter While publishing awbuild.cmd user got Error: socket hang up

2022-08-14T17:43:22Z
Installation and Configuration and Infrastructure

Summary


Details

While publishing awbuild.cmd user got Error: socket hang up

Teamcenter 13.3.0.1,

Active workspace 6.0.1


Solution

Adding additional "timeout" parameter in the config.json file as below, where the value is in milliseconds.

Also different values for this parameter (more or less) will do. Once done restarting the process manager and trying to publish the gateway again will resolve the issue.

Example: %TC_ROOT%\microservices\gateway-1.6.1\config.json


As a note , we don't want an “infinite” or large value here. Pick a value large enough but not too large

KB Article ID# PL8665106

Contents

SummaryDetails

Associated Components

Installation and Configuration and Infrastructure - Active Workspace