Teamcenter Security issue for Oracle Jre 8 u 281 and prior

2022-08-08T09:58:20Z
Installation and Configuration and Infrastructure

Summary


Details

We have Teamcenter 12.2 patch 4 and we are using Oracle Java jre 8 update 281.

As now we have issue with this java version we should move to jre 8 update 291, this seems not compitible with TC 12.2 version.

I tired to update TEM to to use the new Java however it throws an error that it has a missing libraries, and all my services are unable to start, I have reverted back to update 281 then it works fine.

Could you please suggesstions.

Note: we have to stay with TC 12.2 due to TC TIA integration compatibiility, hence upgrading to other TC version is not feasible.

Solution

Answer from development

Any u-version of JRE 8 should work.  We see a problem with u-291+ just when talking with an MS-SQL Server database.  The migration, as the customer noted, went fine without updating the mssqlserver.jar.  That’s because TEM isn’t taking to the database server.  We suspect when you go to add a data model or some other database operation, you’ll run into the problem.  Just let you know that you’ll need that JAR eventually

KB Article ID# PL8664759

Contents

SummaryDetails

Associated Components

Installation and Configuration and Infrastructure - Database