Teamcenter Integration for CATIA V5 (TcIC) Version 12.4.1.16 is available for download by licensed customers at https://support.sw.siemens.com. Go to Teamcenter Downloads and choose CATIA Integration 12 from the 'Select a Version' drop down
TcIC 12.4.1.16 supports CATIA V5 R18, R19, R20, R21, V5-6R2012, V5-6R2013, V5-6R2014, V5-6R2015, V5-6R2016, V5-6R2017, V5-6R2018, V5-6R2019, V5-6R2020 and V5-6R2021 with Teamcenter 11.3, 12.0 and 13.0 or higher versions in those series
Documentation has been posted and customers are encouraged to review the read_me, new features, improvements, closed problem reports
TcIC 12.4.1.16 requires a full deployment, however it is not required to re-deploy the BMIDE template provided that has previously been deployed for the TcIC 12.x release series and Deployment Center is not used
Customers upgrading from TcIC 12.4.1.15 may limit deployment by extracting the CDROM and replacing the following to resolve the issues below
Requiring libcatia (server), Cat2utility.jar (client) and CAA re-build (client)
· PR 10395626 - Save command performance in CatiaV5R18 is bad
CAA must be compiled to support TcIC 12.4.1.16 as part of the deployment and upgrade process