Names of Custom Colors are not available in another installation of Solid Edge

2022-08-02T15:15:39Z

Summary


Details

The user defines some 'Custom Colors' via the 'More...' option that is available in the 'Color' drop-down menu of Solid Edge and gives each custom color a unique name (e.g. User Color #1, User Color #2, User Color #3, etc.).

'More...' option and the available Custom Color names

the defined Custom Colors

naming of the Custom Color

The user then selected these specified 'Custom Colors' to define the color of some elements e.g. in a Draft document.

After saving and closing the Draft document the user opens the file in another installation of Solid Edge and detects that the specified names of the 'Custom Colors' are not available in the other system.

missing User Color #1, User Color #2, User Color #3, ...

Consequently, the user would like to know where these specified names of 'Custom Colors'  are stored and how they can be made available in the other system as well.

Solution

The definitions of the 'Custom Colors' are stored in the following folder of the registry.

Computer\HKEY_CURRENT_USER\SOFTWARE\Siemens\Solid Edge\Version 222\CustomColors\ColorPicker

...\CustomColor\ColorPicker folder with the color and name definitions

The user can transfer these definitions by exporting the selected 'ColorPicker' folder ...

select the folder 'ColorPicker' and choose 'Export' in the context menu of the selection

... defining and saving a registration file name (e.g. CustomColors_ColorPicker.reg) ...

defining and saving the registration file

... and importing this file into the registry of the other system.

Registry Editor > File > Import...

opening the registration file in the other system

quitting the success message

KB Article ID# PL8664122

Contents

SummaryDetails

Associated Components