Selection Intent rule changes for selected sketch in Extrude

2022-08-02T07:14:43Z

Summary


Details

When extruding the sketch curves by using "Sketch Section" in Extrude command, it is created as "Region Boundary Curves" even though "Single Curve" is specified as the selection intent rule.

Reproduced Steps:

1. New part > "Extrude” > “Sketch Section”

2. Create sketch section in Internal Sketch > OK to finish Extrude

            Make sure that “Selection Intent” rule is set to “Single Curve”


3. Edit the extrude feature


Solution

The behavior is working as expected.

Workaround:

If you would like to keep the selection intent (curve) rule, make use of Sketch feature ( an external sketch) rather than the internal sketch.

NOTES/REFERENCES

For features with internal sketch tool such as Extrude, Selection Intent (curve) rule set by Customer Defaults will be applied when created using the internal sketch.


Platforms
Windows x64
10
Release Versions
NX
V1926

*** Please refer to PL8663664 for Japanese article.

KB Article ID# PL8663665

Contents

SummaryDetails

Associated Components