Sheet body not working with 'Automatic' option in "Explosions"

2022-08-02T07:09:21Z

Summary


Details

When creating Explosion, I tried to explode a component with "Automatic" as the explosion type, but if the geometry in the component was Sheet Body, it did not explode.

Reproduced Steps:

1. Prepare a component which has Sheet Body


2. In Assembly tab > Explosions > New Explosion


3. Select the component which includes the sheet body as “Select Component”

4. Select “Automatic” as “Explosion Type” in “Move Components” > select “Auto-explode All” button


Solution

The behavior is working as expected.

Workaround:

Using “Manual” as “Explosion Type”.

NOTES/REFERENCES

For component that is created with a sheet body, "Automatic" option does not work.

Platforms
Windows x64
10
Release Versions
NX
V2027

*** Please refer to PL8663661 for Japanese article.

KB Article ID# PL8663662

Contents

SummaryDetails

Associated Components