JT for CATIA Part does not have the geometrical sets structure, all entities within a part are written into just one node. How to convert the Catia part to JT with geometrical sets structure?
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: PLM_OPEN
Application: TRANSLATORS
Version: V17.0
Function: CATIAV5_TRANS
We need to modify the configuration file for the JT Translator for CATIA.
1. Open ./etc/catiatojt.config with Notepad
2. Change the option PartHierachy from "collapsetopart" to "showopenbodies"
3. Re-generate the JT file, we will see the changes.
e.g.