Example on How to Add Standard Parts Libraries in Solid Edge 2022.

2022-08-01T18:45:05Z

Summary


Details

Example on How to Add Standard Parts Libraries in Solid Edge 2022.

Solution

1. Run the 'Standard Parts Library->StdPartsULibrary.msi' from the Standard Parts Administration machine. Click on the 'Change' button.


2. Select the standard that you would like to add. 'DIN Parts' in this case.


3. Start the 'Database Administrator'.


4. The 'Add Parts from Libraries' should be enabled now. Click on it.


5. Make the selection of the standard you wish to add (ie. DIN). You can be more granular on the choice. In this example all categories under 'DIN' are selected.


6. The image below shows one category expanded showing parts added.


KB Article ID# PL8662824

Contents

SummaryDetails

Associated Components