July 25, 2022
Dear Solid Edge
Customer:
Solid Edge 2022 Maintenance Pack 8 is now available for
download.
We appreciate your continued business and participation
in the software support process - - your reporting helps us make Solid Edge
more productive for how you do business.
Sincerely,
The Solid Edge Team
============
Release Notes:
============
Solid Edge 2022 MP8
Version: 222.00.08.03
Solid Edge 2022 Maintenance Packs are delivered using
Microsoft Installer (MSI) technology.
Support Center: https://support.sw.siemens.com
Solid Edge 2022 MP Download Area: https://support.sw.siemens.com/product/246738425/download/PL20200902110958364
Note: if the MP download area URL doesn't work with your
browser, please navigate from the top-level Support
Center.
======================
Operating System Update:
======================
In addition to the Operating System Requirements
documented in the original Solid Edge 2022 readme,
Solid Edge 2022 MP2 is now certified to run on Windows
11 Enterprise or Professional (64-bit only).
===============
Email Notification:
===============
To receive direct email notifications for Solid Edge
Maintenance Packs, navigate to your Support Center profile:
https://account.sw.siemens.com/profile, scroll down
to Newsletter Subscriptions, then check the box for
Software Field Bulletin.
============================================
This Maintenance Pack
addresses the following PRs:
============================================
===Assembly===
PR 10362412: features cannot be selected in the graphics window while
using 'Edit In Place'
PR 10310996: Feature "Pattern" toolbar changes to "Along
Curve."
PR 10376801:
Performance issues while editing a feature and not making any modifications
PR 8602660:
Cannot place pipe and fitting in the XpresRoute environment
PR 10367694:
impossible to migrate Standard Parts to version 2022
PR 10386700: Wire
command - center point option not locating all rectangular faces
PR 10305959:
Locate issues in Profile while IPA
PR 10363385:
performance issues on opening this file
PR 10366854:
Fixed a performance issue while editing assembly features
===Draft===
PR 10149215: FOA
drawing views not being correct after saving all members in the FOA file, then
updating the drawing views
===General===
PR 10304484:
Can't copy Sketch with conical curve created in Draft to part or PSM files
PR 10320865:
Getting unwanted behavior in Profile Text
PR 10359794:
Custom File Properties disappearing
PR 10361042:
Match coordinate system (new version) doesn't support linked mate
===Teamcenter
Integration for Solid Edge===
PR 10336549:
Standard Parts PMSX file not accessible
PR 10371388:
Aborting while creating a manual connector
PR 10372246:
Synchronize virtual components does add duplicate structure
PR 10379071: JT
Options revert to default
===Translators===
PR 10307286:
Abort while setting templates & materials while "Publishing Internal
Components."
PR 10341693:
opening STP with and without 'create Internal Components' differs
===Technical
Publication ===
PR 10229046: 3D
Publishing: move parts CTRL selection in exploded mode
PR 10388262: 3D
Publishing crashes when saving a document