Oracle has released a quarterly Critical Patch Update to fix vulnerabilities in Oracle database products: Oracle Critical Patch Update for July 2022 .
These patches are available for download by licensed customers at https://support.sw.siemens.com
The patches include:
Oracle 19c (19.16.0.0.220719)
p34133642_190000_Linux-x86-64.zip
p34133642_190000_Solaris86-64.zip
p34110685_190000_MSWIN-x86-64.zip
Oracle 19c Opatch (12.2.0.1.32)
p6880880_190000_Linux-x86-64.zip
p6880880_190000_MSWIN-x86-64.zip
p6880880_190000_Solaris86-64.zip
Teamcenter supports these versions of Oracle Database:
For the latest information, please refer to the Teamcenter Platform Matrix
at Support Center. It is located under Support White Papers under Teamcenter
Download.
Oracle 12c - Teamcenter 10.1.5, Teamcenter 11.x, Teamcenter 12.x
Oracle 18c - Teamcenter 11.x, Teamcenter 12.x
Oracle 19c - Teamcenter 12.4.x, Teamcenter 13.x, Teamcenter 14.x
Note1: Oracle 12.1.0.x is out of support as of 19-Jul-2019 and no additional patches are
posted for this version.
Note2: Oracle 18c is out of support as of 30-Jun-2021 and no additional patches are posted
for this version.
Note3: Oracle 12.2.0.x is out of support as of Jan-2022 and no additional patches are
posted for this version.