Teamcenter Visualization File > New missing options in TcVis Professional 13.3

2022-07-21T14:56:39Z
Lifecycle Visualization

Summary


Details

We installed TcVis Professional 13.3 and when we open it and go to File > New we only see an option to create an animation.

When we used TcVis Professional13.1 we also saw options to create a Technical Illustration, Technical Portfolio and a Process Document. How do we add the other three options to the newest version?

Solution

This issue was resolved after the customer went to Add/Remove Programs and found TcVis 13.3. The selected it and clicked on Modify then clicked on Next > Next. On the Custom Setup screen they expanded Professional and saw that they didn't install the optional modules called Visualization Illustration and Variation Analysis.

Notes

KB Article ID# PL8659088

Contents

SummaryDetails

Associated Components

Visualization