Solid Edge SEDM where used pops up when using "Open Draft"

2022-08-25T10:27:02Z
DOC_MANAGEMENT

Summary


Details

Since Solid Edge 2022 MP7 Solid Edge Data Management (SEDM) throws up a "Where Used" window every time you use the "Open Draft" button even though the vault location is correctly defined and the location has been indexed.

Clicking "Next" opens the draft without any issues since the draft is located in the vault and the vault has been indexed, but it is an unnecessary step and users are being confused by this window.

How do we return to the default behavior?

Solution

This is a backport of a Solid Edge 2023 option. In Solid Edge 2023 this will be an option in the Manage options and options.xml.

As a workaround you can return to the "old" behavior by changing a regkey:

HKEY_CURRENT_USER\SOFTWARE\Siemens\Solid Edge\Version 222\Global\SEDM_PromptBrowseDialog to "0"

Notes

Notes

KB Article ID# PL8658442

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEDM