TC 12.2
TC 13.2
Description:
I am looking to create 2 LOV's where LOV 2 is dependent on what was set in LOV 1.
LOV 1
-70001 Pump Type
LOV 2
Attributes
1145 Pump Type (-70001)
1146 Pump Size (-70002)
I am trying to make the attributes dependent on each other.
Solution
Please find below the steps I used to create the cascade LOV.
1- Go to KeyLOV and click on "Create a New Instance"
2- Enter an ID for the KeyLov that starts with a negative number
3- I named the top LOV (header) as "PUMP"
4- Then selected "PUMP and added one submenu called "A:PUMP Type"
5- Under "A:PUMP Type" added three submenus and named them
A1: Pump X
A2: Pump Y
A3: Pump Z
6- Then I kept adding a submenu under each Pump type
7- Then, under each Pump Size I added "Add Entry"
and named the entries as follow:
8- Save it
And when it is time to classify, it works as expected :
Notes
Notes