Solid Edge Electrical Manager shuts down when you launch SEWHD

2022-08-01T18:37:23Z
APPLICATION

Summary


Details

Electrical Manager shuts down when you launch Solid Edge Wiring & Harness Design.

Solution

Review of the EletricalManager logfile contains the message:

java.net.BindException: Address already in use: NET_Bind

It also show the default port: 49901

When everything starts correctly you will see:

   Solid Edge Electrical Integration Server started on non secure port 49901

So, everything indicates a possible port conflict or hijack.

First, try a reboot to see if it resolves the conflict. If the conflict persists you can use the Resource Monitor Network tab to see what application is using port 49901:


Once the hijacker process is stopped you should be able to restart Electrical Manager.

Notes

KB Article ID# PL8655618

Contents

SummaryDetails

Associated Components

APPLICATION: SE_ELECTRICAL