Process Simulate does not open

2022-07-13T21:11:57Z

Summary


Details

Process Simulate does not open at all.
Process Simulate does not launch.
Process Simulate closes itself right after launch.



Solution

- Make sure your graphics card is up to date. 
- You should install all related hotfixes from each version. If you have multiple versions, make sure the Tecnomatix Version selector is set to the the relevant version when doing so.  
- If you have multiple versions the shortcut launcher should have these bold directories into the TecnomatixShared directory, (and the directories should already exist). Anything not in bold should be fine with whatever values you already have. 
C:\....\TecnomatixShared\TecnomatixCurrent\eMPower\Tune.exe /c NewAssembler /l offline
- If none of the above helps, it would be better to uninstall, then install making sure you run the installer as an administrator



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V17.0
Function: SETUP

Ref: 001-10386738

KB Article ID# PL8654982

Contents

SummaryDetails

Associated Components