Why Maintain Associativity option is disable?

2023-01-25T10:45:58Z

Summary


Details

Facing issue while using the project sketch command to project sketch.

When user trying to project sketch "Maintain Associativity while projecting geometry" option gets disabled.

Solution

It is obvious , that the inter-part Links point to another assembly.

An Inter-part relations may and cannot be established, when the Assembly is a Family of assemblies, because a link only will point to the part in an assembly, but not a member.

Notes

10336786

KB Article ID# PL8654945

Contents

SummaryDetails

Associated Components