When running prepare.exe on an NX file, no file creates and the error above shows up.
Opening the same file in Teamcenter Visualization mockup shows an error, too.
Solution
This is because of missing CGM datas not stored in the NX prt.
To correct this:
- Open the prt in NX
- "File > Options > Save Options"
- Switch on "Save Drawing CGM data" and Save the prt file
Now the file translates fine preview .exe
Notes
PR 10380082