How to clean duplicate entities from imported dwg/dxf ?
Solution
It is possible for a sketch to have redundant geometry consisting of identical superimposed elements. Duplicate sketch elements can cause undesirable effects for further processes that use the sketch geometry. Non-native geometry imported into Solid Edge, such as data originating in DXF and DWG file formats, sometimes import with duplicate and overlapping geometry. "Clean Sketch" command is used to move or delete redundant and unwanted elements from the sketch.
Valid input for identical elements are:
• Point elements
• Lines
• Circles
• Arcs
• Ellipses
• Partial ellipses
• B-spline curves
Notes
Notes