If you have 2 components, A and B in an assembly: Component A has a sketch with 2 circles, and you want to project only one circle into component B surface, but NX selects both circles, how can you accomplish this task?
SolutionWhile in Project Curve command, set the selection filter
to Curve and Entire Assembly, then change the middle filter on the screen from Infer
Curves to Single Curve then you can select a single sketch curve.
Notes