How do you to create MBD FCF callout for multiple counterbore holes of the same size

2022-08-30T14:38:49Z

Summary


Details

How do you to create MBD FCF callout for multiple counterbore holes of the same size?

Solution

You can create FCF callout using MBD Logical Rules in Reuse Library as below:

First using MBD Logical Rules out of the box from Reuse Library to create a Datum attach to any face of the part.


Then create FCF from MBD Logical Rules--> Select “Create Position from” to select the datum plane with the options as below:


The result is as below:


Notes

KB Article ID# PL8654721

Contents

SummaryDetails

Associated Components