Exporting column formatting from property manager

2022-06-30T15:06:30Z

Summary


Details

Is it possible to get the columns added in Property Manager to show up in the same arrangement for other users? 



Solution

Yes, the easiest way to accomplish this is to use the Settings and Preferences Wizard to copy user settings from one machine to another or one user to another. Be aware that this copies ALL of a user's settings and preferences. 

The specific location in the registry which stores column settings is the following: 

Computer\HKEY_CURRENT_USER\SOFTWARE\Siemens\Solid Edge\Version 222\General\PropertyManager


So as an alternative, you could go to this location in the registry editor and Export this key. This will create a registry file with just this information in it. Then each user will double-click on the registry file, which will issue a Microsoft warning that the file is about to make changes to the registry and ask if you are sure this is what you want to do. Say Yes or OK and then you should get a secondary confirmation message that the changes were made. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V222.0
Function: OTHER

Ref: 001-10379376

KB Article ID# PL8653899

Contents

SummaryDetails

Associated Components