NX Unable to export routing object (.plmxml) from Teamcenter Integrated NX

2022-11-30T22:20:16Z
NX for Design

Summary


Details

Unable to export routing object (.plmxml) from Teamcenter Integrated NX.

While working in the Electrical module in NX, the import/export option is not working properly while running from NX.


Solution

As per the above snapshot in the Capital, it appears to be missing "bundles", which are called "topology" in NX Routing.

 

There are a couple of customer defaults that control whether topology is exported or not. The customer may have to enable the said customer defaults. See the below snapshot-


Note: These options are applicable for both Native NX and TCIN.

Notes

8572394

Notes

KB Article ID# PL8653856

Contents

SummaryDetails

Associated Components

Routing