Solid Edge Solid Edge cannot connect to Teamcenter AWS Cloud environment.

2022-09-26T18:46:45Z
DOC_MANAGEMENT

Summary


Details

When trying to connect Solid Edge 2022 to a Teamcenter 13.3 cloud environment an SSL certificate error occurs:Runtime Exception: Failed to encrypt/decrypt the service request.

SSL certificate problem: self signed certificate in certificate chain...

Solution

If the environment variable TEAMCENTER_SSL_CERT_FILE is not set when running SEEC in the Teamcenter Secure Socket Layer (SSL) this error will occur.

Set the variable to the same certificate file that is used for Teamcenter SSL setup. Ensure you use the fully qualified host name in the URL for the connection. TEAMCENTER_SSL_CERT_FILE=.pem) and path> Notes

Notes

KB Article ID# PL8653414

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC